Execution


What you will find in this section:

  1. Execution
  2. Related topics

 

Firmware update

The device provides a function for updating the firmware. New versions can contain bug fixes, optimize the performance and expand the functionality.

Update files are provided by Phoenix Contact GmbH & Co. KG. The respective update containers can be downloaded from the product-specific pages at phoenixcontact.com.

 

Execution

 

Execution of a firmware update
Execution of a firmware update

 

Firmware update

In this area, you can load a new firmware update onto the device. To perform the update, you need administrator rights.

An update can only be performed via the web server of the device.

File

Upload the new firmware file. Click the “Upload” button to begin the process.

 

Progress and state
Progress and state

 

Progress and state

Once the firmware file has been uploaded, you can start the update on the device by clicking “Perform update”.

 

Observe the following when performing a firmware update:

  • The update process can take several minutes and should not be interrupted.
  • Do not exit the subpage for updating the firmware of the web-based management.
  • During the update process, the device restarts and is thus unavailable for a certain period of time.
  • During certain steps of the update process, it is possible that the energy meters of the system are stopped.

 

  1. Security

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history